Motor_Poles
Motor_Poles
| Address: | 4135 (1027H) |
| Type: | WORD |
| Access: | Read/Write |
| Unit: | # of motor poles |
| Range: | 50; 100 |
| Default Value: | 50 |
| Store Supported: | Yes |
| Description: |
It sets the number of motor poles. The number of poles can be computed as follow: Take the Step Angle value from motor data sheet (typically 1.8°) and then perform the following computation: For a motor with Step Angle = 1.8° the number of rotor teeth is 50. |
| Notes: |
This object can only be set with the motor at a standstill. If the value set is not valid the default value is stored. |